Questions about posting

Thank you for your continued support.

Regarding the MPQ4242GVE-0000-AEC1-Z that we have purchased from your company, we contacted you to request a technical confirmation regarding the specifications of the ONE TIME PROGRAM (OTP) function.

Currently, we are checking the following description in the datasheet.
Bits Name: D[7] OTP_PROGRAM
Default: 0x0
Description:
Configures the I2C register value into the OTP memory cell.
A password is required before using the OTP.
The OTP can be configured once. Only the MPQ4242-0000 and
OTP_PAGE = 0 can be used to configure the OTP.
Write 1 to this bit to implement OTP configurations.
After configuring is complete, this bit automatically resets to 0.
Apply a 12V VIN while configuring the OTP.

In the above description,
“A password is required before using the OTP”
is written, but

  • the specific content of the password
  • the setting method (registers, sequence, etc.)
    are not described, and we have not been able to confirm them.
    Therefore, we would like to ask you the following points:
  1. The specification and setting method of the password required when writing OTP
  2. The procedure to fix the initial value (I2C register value) using OTP
  3. Precautions during execution (voltage conditions, method to check writing, etc.)

In order to consider settings with mass production in mind, I would like to understand the method to reliably fix the initial values. If you have any manufacturer documents or application notes, I would be grateful if you could provide them. I apologize for troubling you during your busy schedule, but I sincerely ask for your confirmation.

Hi @hirosawa,

I believe this thread is related to a more recent thread of yours that I replied to: Specifications of the ONE TIME PROGRAM (OTP) function of MPQ4242GVE-0000-AEC1-Z - Other Products - Monolithic Power Systems’ Technical Forum

We can continue in the linked thread instead of this one.

Thanks,
Rubas