Is it possible to supply an external power supply (24v) in a similar fashion to the MP8007/8?
The MP8017 reference design shows a 10uH inductor between VBUS and the transformer, where the datasheet example circuit doesn’t. What is the purpose of the inductor and how does that affect the inductance value of the flyback transformer?
Yes, you can use external power supply with MP8017.
The combination of capacitors and inductor (C1A, L1, C1B) forms a pi-filter. It is ensuring that the input to the transformer is clean. If you verify the Vbus output is clean, you can directly connect Vbus to transformer. L1 inductor does not affect the inductance of transformer.
Please refer to the other post of yours. I’m sorry I misunderstood but MP8017 will not be able to work with 24V adaptor supply.
Kindly keep all your questions in one post in the future to avoid getting flagged by the system.
I’ll be closing this post and keep the other one active.