Why does the MP024-10 an overvoltage exceeding 700V at the drain pin? Where did I make a mistake in my circuit design?

The circuit design was tested by plugging it into the same outlet as a blender. It was observed that when the Pulse button on the blender was pressed, the voltage at the drain pin of the MP024-10 IC reached 849V, which caused the IC to fail.
The points I would like to know are as follows:

  1. The circuit board design was not in use; it was merely plugged into the same outlet as a 1000W blender. Does the interference come from the blender, and what type of interference is it?
  2. Where in the circuit design is incorrect?
  3. What could be the causes of the voltage exceeding 700V?

Additional information:

  1. Testing with an ELCB also showed overvoltage exceeding 700V, but it occurred less frequently compared to the test with the blender.
  2. The circuit diagram can be found in the attached images.

Based on the circuit design, is there a solution or approach to fix this issue?

The voltage waveform exceeding 700V at the drain pin of the MP024-10 IC.

So you have some crazy amount of distortion and noise on the incoming AC line? Created by a blender and this has induced a malfunction during turn off. Does the physical proximity of the blender matter or is it simply a case that it has to be on the same plug. What is happening to the output voltage during this malfunction.

I would say you are testing this application circuit more rigorously than anybody else. Is the blender a cheap stand in for a more defined line side IEC test.

1.It is simply a case of being plugged into the same outlet.
2. The blender’s power cord complies with the 60227 IEC standard.
3. We previously tested a circuit using the IC MP020-5 in the same way, but no overvoltage was observed at the drain pin.