Dear Support member.
I’m using MPM3695-25 with Virtual Bench PRO4.0
Please tell me about 25h register and 26h register.
Q. what is mean 25h register and 26h register.
I set “Voltage setting” is 0.72V and “Vout Scale Loop” is 0.333.
(I use external divider.)
I must set “Vout margin High” and “Vout margin Low”.
but I don’t know those registers mean.

Hi Ryota,
The Vout Margin High/Low are to check for functionality at extremes of operating tolerances. It is mainly used in reg 01h found on page 35 on the datasheet.
If an output overvoltage warning or output OV fault is detected when the output is margined high, the part ignores the condition and continues to operate without interruption depending on the operation command. The same happens for when it is margined low.
1 Like
Dear Cecilia
Thank you for answer.
I’m just checking.
Is this Vout Margin High/Low works of alert function?
Best regards.
Hi Ryota,
The Vout Margin High/Low do not have an alert function but the VIN_OV_FAULT_LIMIT will trigger and alert you that there is a fault when there is an over-voltage condition.
1 Like
What’s the difference between the 'Margin High(ignore fault)‘and’Margin High(act on fault)’?
i’ll appreciate that if you give a more detailed explanation.
Hi Cecilia,can you explain the question i send just now,thank you very much.
Hi Cecilia,do you receive the question i sent to you?We just use the mpm3695-10 in my design,but it seems that i can not understand this question,Hope you can reply as soon as possible,thank you very much