What is the best topology for DCDC power converter with the following specs:
DC in, min 30V, DC in, max: 110V, Isolated Output: 15V 10A
What is the best topology for DCDC power converter with the following specs:
DC in, min 30V, DC in, max: 110V, Isolated Output: 15V 10A
Hello,
In general for DCDC isolation, I think a flyback could work. Here is information on this topology.
An Introduction to Flyback Converters: Parameters, Topology, and Controllers | Article | MPS (monolithicpower.com)
For 150W power, you could refer to our ACDC flybacks.
Best Regards,
Yu