Use MPQ4436A as an adjustable, constant current source

We would like to use the MPQ4436 as an adjustable constant current source (preferably with two in parallel to increase the total available output current). Do you have any suggestions on implementing an adjustable, constant current topology on the MPQ4436A?
If not, are there any automotive qualified iC’s in your portfolio that could provide an adjustable, constant current output of approximately 0-10 amps at Vin=5V, Vout about 3V?
Thanks.

Hello,

The MPQ4436A is constant voltage buck. For a constant current buck, I would recommend a buck from our automotive LED driver families.

I hope this helps.

Eliza