Support Request for Custom Transformer Design – MPQ18913

Hi,

I am designing an isolated DC/DC converter for 24V input and 24V output with a maximum output power of 5W. To achieve very low primary-to-secondary interwinding capacitance, I have selected the MPQ18913 controller.

I have purchased the EVQ18913-D-01A evaluation board along with several toroidal ferrite cores to build a custom transformer. The transformer used on the EVK board is well designed; however, it reaches temperatures above 50°C at just 3W load. Therefore, I would like to use a slightly larger core to achieve cooler operation.

To keep the BOM cost as low as possible, I prefer not to use a stock transformer.

I am attempting to replace the EVK board transformer with my own custom-wound transformer along with a suitable resonant capacitor. However, I have not been successful despite multiple attempts using different cores.

Below is the list of cores available with me for testing. I kindly request MPS to suggest a suitable core and the recommended turns for my application.

B64290L0038X087, B64290L0038X830, B64290L0044X830, B64290L0644X830, B64290L0044X027, B64290L0038X035, B64290A0044X087, B64290L0038X037, B64290L0742X087, B64290L0658X087, B64290L0044X049.

Thank you for your support.

Best regards,
Udhay

Given the following specifications that you have listed, I would implore you to evaluate the MID6W2424A module that integrates the transformer in the package.

It is capable of 6W with a 24V input where the integrated transformer is 1:1 which would yield you 24Vout with no problem. The level of isolation between the primary and secondary is 3kVRMS and is EN62368-1 Compliant.

This should save on the design, space, and operates between -40°C to +105°C Operating Ambient Temperature (TA) range.

Best,

Krishan

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.