Setting Output voltage for MPM3695-100 device

I have a question about setting the output voltage of the MPM3695 device.
MPM3695-100-0001 will be mounted on the board and the Vout=1.0(V) feedback resister in table 6 of datasheet will connected.
If the CTRL pin is set to High、Which the output voltage of VOUT pin is A or B ?
A: 1.2V (Register Code=21h default value)
B: 1.0V

Hi @gotou.yoshitsug,
The CTRL pin is used only to turn on(High) and turn off(Low) the regulator. So, in this case it will be 1.0 V.

Hope this helps.

Best,
Saquib

1 Like