Request for Design Recommendation – 150W Isolated Power Supply

Hello Team,

We are currently developing a low-cost, compact, isolated design with auto-grading capabilities, and we’re using the LM5185 controller in our initial prototype.

However, we would like to confirm whether this design can be scaled to support up to 150W output power with the following specifications:
Input Voltage: 24V to 100V
Output Voltage:15V
Output Current:10–12A
Output Power:150W

If the LM5185 is not suitable for this power level, we would appreciate your recommendation for an alternative solution that meets our requirements.

Thank you for your support.

Best regards,
Vandana D

Hello, welcome to the MPS Forums.

Here are some parts that I can reccomend for this application:

I suppose there are compromises with all of these ICs, but I figured I would show them here for evaluation in case something here works.

Best,
Krishan

Dear Team,
Since the system is battery-powered, we are not aiming for high input wattage. Instead, please suggest a solution that offers low input power with high output efficiency, based on the following requirements:

Input Voltage:24V to 100V
Output Voltage:15V
Output Current:10–12A
Output Power:150W
Looking forward to your suggestions.

Regards,
Vandana D

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.