To whom it may concern.
I’m Shinichi Yamamoto.
I have a question about the MP3301GJ.
We can see LED Current Programming section on page 8 shows PWM max fewquency is 1kHz.
A question is regarding the acceptable PWM frequency of 1kHz.
What is the maximum usable percentage increase for a 1kHz frequency?
Can be 10% increase(1.1kHz) recommended?
Hi Shinichi,
Thank you for posting on the MPS Technical Forum.
According to the datasheet, you can use a PWM frequency above 1kHz as long as you include an RC filter with a cutoff frequency less than the PWM frequency divided by 10.
What PWM frequency are you hoping to use? 1.1kHz?
Best,
Allison
Hi Allison
Thank you for your replay.
I want to drive the MP3301 at 1kHz, but due to variations, the PWM frequency may rise to 1.1kHz. I would like to ask if this 1.1kHz is acceptable or even recommended as a PWM frequency.
In this case off cource, is 1.1kHz drive available by not using cutoff filter ?
Hi Shinichi,
You should not need the RC filter.
Just to be safe, what is your PWM duty cycle range?
Thanks,
Allison
I’ve not decided dimming range yet.
The datasheet states that for PWM dimming, the DC voltage should be between 0.7V and 1.4V. Since I have 3.3V available for PWM, I’m considering using a duty cycle setting of 20% or higher. Is this possible?
Hi Shinichi,
Yes, this is possible.
To confirm your first question, you do not need an RC filter.
Best,
Allison
Thank you for your response.
I understand the content.