Protecting the input voltage to the DC/DC from short to gnd

Hi

using the MPQ8775AGVE:

The question is what happens if pin SW1 or pin SW2 is suddenly shorted to GND?

Does the chip have a protection mechanism for this senario?

Best Regards

Alon Shemesh

The MPQ8875 has a peak/valley current mode control scheme, which means that it monitors the inductor current at the SW node. In theory, a short on one of those nodes to GND should be recoverable if the current limiting acts fast and turns off the internal FETs before damage occurs. In practice, this has not been sufficiently tested, and we cannot guarantee that the device will survive a short on either SW pin to GND.

A direct SW-to-GND short is a hard fault, not just an output overload: when the high-side FET turns on it can tie VIN to GND until the current limit reacts. Cycle-by-cycle limiting and thermal shutdown may help, but without a guaranteed test they should not be the only protection. An input fuse or eFuse rated for the fault current is the usual external backup.