Pre programmed PD charger IC with built-in buck boost driver

Hello team,

Please suggest a Power bank SOC(for wireless charger), that is pre-programmed and has built in buck boost IC.We will be using Li-Po 3.3V to 4.2V battery. it should automatically adapt to QC,PD protocol.

Thanks and regards.

Hello, welcome to the MPS Forums!

Perhaps you can start your search with the following buck-boost charger IC:

MP2651 | I2C-Controlled, USB PD 6A Buck-Boost Charger with OTG/Source Mode for 1-Cell to 4-Cell Series Battery Applications | MPS

This is a versatile option that can work; however the input range here goes from 4V - 22V.

Dear Sir,

Can we get technical support in using MPS IC for power bank(uses DRP mode,Li-Po battery) and wireless charger applications(sink mode uses Lead acid battery). We want guidelines in configuring IC.How can we contact, is there any separate mail id.

Thanks and regards.

Hello again,

Please submit a ticket to receive more in-depth design assistance via email in that case:

Contact MPS - Design Assistance Contact

I’d also encourage you to see the following in the meantime while the ticket processes:

Chargers - Battery Management - Products

Let me know if there are any email delays in contact in this thread.

Best,

Krishan