Please clarify the externa ramp for low ESR on MP8771

At the top left section on page 18 it is mentioned that an external ramp (Rramp and Cr) is needed when using low ESR capacitors.
Please provide details on how to connect and calculate Rramp and Cr.

Also on page 17 the feedback network contains Rt and Cf. Please clarify the purpose on these.

Finally I found an error in the datasheet. On page 15 the pin 15 is described as “No connection. NC must be left floating.”.
But in the layout in page 19 the pin 15 is connected to pin 14.

Hello @tomas.tollemark ,

The MP8771 has an internally generated ramp which will keep it stable. If extra stability is required, then an external ramp can be added to supplement the internal one, but this is not needed except in special cases.

As for the diagram on page 17 Rt is the Thevenin resistor that exists to increase the effective resistance seen in series with the FB pin. Doing so has benefits to the control loop. Cf is the feedforward capacitor and it is used to adjust the phase margin of the control loop. We have an article that explains how these two components modify the control loop that can be found at this link.

I double checked with the product expert and the NC pins 1 & 15 can be left floating or can be connected to VCC or GND. The part will work the same in any case.

Best Regards

-Kerr

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.