Not working GUI MP2722,MP2651 in Windows 10

Hi, I need to evaluate GUI MP2722 and MP2651, but on two very different laptops with Windows 10 I cannot get it working. On both laptops I can start GUI application, it shows Device Connected but everytime I click on any button (Update All, Read All or Reset All) the application crashes in 2-3 seconds. I tried Run as administrator or Run in compatiblity modes (win8, winXP…), perform several restarts but with no luck. Have you got anybody any advice? All EVB are working fine.

I have these EVB: MEZS7-PDPowerbank-MP2651, MEZS7-1s-4spdpowerbank and EVKT-mp2722

Hi,

Does your EVB have any problems when your GUI application crashed? If it is all good, check the I2C connection first and I guess probably there is a problem with the software download. You can contact MPS and we can send you the GUI Software. Download again and try.

Please fill out the MPS NOW Technical Support form. Tell them you need MP2722/MP2651 GUI software. A member from the MPS NOW team will contact you within 24–36 hours about this request.
Contact MPS - Contact

Best,
Fox

Im really sure I2C connection is correct and reliable. Okay, will try to download it once again but both applications installed fine without any errors. IMHO if the installation files would be corrupted or uncomplete, then installation wouldnt finish successfully. But I will give it a try.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.