Need transformer for 8009A design

I’m looking for a POE 802.3at design that is 37V to 57V in and 5V 3A out (the
power draw is 9W nominal but can go up to 15W for 50ms). I need the transformer
to be under 13mm height. I believe the MP8009 would work but am open to
suggestions. I would like the efficiency to be above 85% with a goal of 90%. I
cannot use the one in the kit because it’s sourced from a chinese company.

I have located a transformer that could work for our design: FCT1-50M22SL | Power Converter Transformers | Coilcraft can I get some design help since there are no tools (simulations or web tools) to design this transformer into the MP8009?

Hello Steven,

Please see the email thread where we have been working with you. I sent over some design tools to help you with your project.

Best,
-Kerr

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.