We are currently developing a 3-phase BLDC motor driver using MSP6531 as gate driver.
However, the issue we encountering is that the motor triggers the OCP protection of the MPS6531 as soon as it starts.
1.We attemped to short the Rsense R5 directly to ground, but the protection was still triggered. The protection is only avoided when OC_REF pin is directly connected to GND.
2.The protection is particularly prone to occuring during startup; once the motor is running, the issue no longer occurs.
3.Using a current meter, the measured peak current did not exceed 10A, ruling out the possibility of MOSFET shoot-through.
4.The Vg signal of Q1 and Q2 were probed, and the waveforms are as follows. Severe ringing is observed during startup.
ch1: Vg of Q2
ch3: Vg of Q1
ch4: Vs of Q1
reference schematic
Please provide us with some suggestions
Regards