MPS2918GL: Clarification on Internal Regulator Behavior at VIN < 6V

Hello,
I am using the MPS2918GL as a buck converter with an input voltage range of 5.5V to 17V. According to the datasheet, the internal regulator operates when VIN is 6V or higher, while the regulator output voltage is specified as 4.5V to 5.5V.
It appears that, even assuming a 0.5V dropout at a 50mA regulator load, generating a 5V output from a 5.5V VIN should still be possible.
Could you please confirm whether the converter is expected to operate correctly in the VIN range between 5.5V and 6V? I do not have another voltage source available to supply VCC2.

Thank you

Hi @grenadem ,

Are you referring to the MP2918?

As long as the converter is supplied with the recommended input voltage between 4V-40V it will operate correctly.

Thanks, Will

Hey @william.snyder

yes im referring to mp2918