I would like to know the I2C Value of the MPQ8875AGVE-0000-AEC1 part.
Is it the same as the I2C Default Value written in the datasheet?
Hi,
If it is a new IC, it should be the same as the I2Cd default value written in the datasheet, You can also use GUI to read the value.
Best,
Fox
I received a sample MPQ8875AGVE-0000-AEC1 from my dealer. I replaced the EVQ8875 with the ‘0000’ code part and read the I2C value. However, the I2C value matched the one in the EVQ8875 datasheet, not the one in the MPQ8875AGVE-0000-AEC1 datasheet.
Did I receive the wrong sample? Should I buy it from Mouser and try again?
These questions arise because the dealer informed me that the default value in the datasheet cannot be used.
I want to use the MPQ8875 with the default value applied.

The picture above is the I2C Value of the “0000” Chip received from the dealer.
Hi,
I think if it is not the same, you can use GUI to do a non-volatile write to any value you want to have. It is a MTP product, so you can do a non-volatile write.
Best,
Fox
Thank you for the reply.
What I want is to purchase the MPQ8875 chip with the default value in the datasheet applied.
If I purchase MPQ8875AGVE-0000-AEC1, does the default value in the datasheet apply?
If not, wouldn’t the datasheet need to be modified?