Hi,
I have a design with MPQ8875A converter. I have watched in its datasheet, in “ABSOLUTE MAXIMUM RATINGS” paragraph (page 7) that the maximum voltage for this pin is 5,5V (All other pins … -0.3V to +5.5V)
BUT in several examples of design (pages 63, 64), it has a Pull-Up to VIN (up to 36V).
I would like to clarify the maximum voltage that I can apply to EN pin.
Hello @jjvv ,
The EN pin will be able to handle up to the abs max of PVIN, 42V. The evaluation board shows a design with the MPQ8875A that has been tested, so as long as Vin is within the recommended range it can be used as a pull up for EN.
Apologies for the confusion from our end regarding EN maximum voltage.
Hope this helps!
Regards,
Jonathan
Ok, thanks for your answer!
Thanks. Hope MPQ8875A datasheet updated soon.
I would be surprised if it didn’t blow up. The eval board shows also a current limiting resistor.
Typically the EN pin has a 6V ish ESD protection device like a zener on it. If you apply high voltage from a low impedance source it will blow, if you apply high voltage through a current limiting resistor the EN pin will sit at 6V or so the part will operate and not blow up.