Hi,
We are using MPQ8633B to generate 3.3V on our board. The specs are as follows:
Vin = 12V
Vout = 3.3V
Iout = 13.5A
Output inductor DCR = 2.53 mOhm
From our calculations, it seems around 2.5W will get dissipated across the converter and around 0.5W across the inductor.
Kindly confirm the following:
- Is the calculation correct?
- If yes, then can the package handle 2.5W of power across it (as the max. power dissipation is not mentioned in the datasheet)?
Awaiting an early response for the same.