Hi, I have problem to program a MPQ7920-003 device on the eval board. The ENTER_MTP_MODE bit can not be set to 1 probably because the password is not correct ?!? What is the default password for MPQ7920 ???
Thanks in advance for your support
Pierre
Hi p.stassain,
Let me look into this.
Thanks,
Cindy
Hi p.stassain,
Version -0003 is not MTP programmable, only -0000 has a two-time programmable MTP. Please see *Note 1 in the datasheet.
Thanks,
Cindy
Hi Cindy, as far as I understand, MPQ7920GRM_0000 is MTP so it is 2 times programmable.
while the MPQ7920GRM-0003 is already 1 time programmed soi it is OTP (1 time programmable).
So please could you give me the MTP password for the chip MTP7920GRM- (0000 or 0003) ??
Thanks in advance
Pierre
Yes, -0003 is 2x programmable and -0000 is one. The MTP program password is “mps0519”.
Cindy