Hello,
We are setting up CAN communication between an MCU and the MPQ7225A LED driver:
At 500 kbps or lower: The LED driver responds normally with status and CRC.
At 1 Mbps or higher: There is no response at all.
What potential causes should I look into? Could PCB layout (artwork) be the main suspect, or should I re-evaluate physical layer factors like termination resistors and CAN signal integrity?
Hi Nobleman1225,
Thanks for reaching out, the below is our recommended debug sequence:
-
Scope the differential signal at 1 Mbps. Check V_DIFF, edge times, and ringing.
-
Measure DC resistance between DATA+ and DATA−. Confirm ~120 Ω (single termination).
-
Check TJA1057 configuration: baud rate, sample point, slew rate, termination enable.
-
Inspect PCB layout: trace length, reference plane, capacitance, ESD component placement.
-
Verify MCU CAN clock accuracy (±1% or better).
-
Check decoupling on both V_CC rails.
If the differential signal looks clean on the scope but the MPQ7225 still doesn’t respond, the issue is likely in the sync byte timing or CRC calculation on the MCU side. In that case, capture the raw DATA+/DATA− waveform and decode it byte-by-byte to identify where the frame breaks down.