Hello there, i have an MPQ6626 on a custom board and i am trying enable all 6 channels of the 6626 via SPI. I have gone through the datasheet but do not know what command to send via SPI to achieve this. Bear in mind, i have tried a few things including writing 0x9FFE which is meant to enable SRR and all the channels but i didnt get any result.
Please help with a sample code/snippet of how i can achieve this or command/data format. Thanks
Hello,
Please refer to the data transfer and serial interface section on page 12 of the datasheet.
You can also play around with our evaluation board and utilize our GUI to start off.
EVQ6626-F-00A | 40V, 0.8A, Hex Half-Bridge Motor Driver with Serial Input Control Evaluation Board, AEC-Q100 Qualified | MPS (monolithicpower.com)
If you need additional assistance, please submit a ticket through MPS NOW Remote Support - Support.
Best Regards,
Yu