Hello
Thank you for your support.
I intend to use MPQ6527 in parallel.
For example,…
・Use case1:
Use OUT1 and OUTx individually. up to 800mA each.
・Use case2:
Tie OUT1 & OUTx in parallel. up to 1600mA.
Question
There are 10-half bridge inside , but is over-current limit same for all OUT1 to OUT10?
Foe example
If OUT1 over-current limit were 2.5A (max value) , then OUT2~OUT10 is also 2.5A?
If OUT1 over-current limit were 1.0A (min,value) , then OUT2~OUT10 is also 1.0A?
Please advise.
Best Regards