MPQ4323MGQCE-AEC1-Z Conducted Emission Test Observations - CISPR25 Class 5 Limit

Hello MPS Team,

We are currently performing CISPR25 Class 5 conducted emission testing on our DUT and observed some emission concerns that we would like your guidance.

The DUT uses MPQ4323MGQCE-AEC1-Z buck converters for 3.3 V and 1.8 V generation. The overall power architecture is based on MPS buck converters and LDOs.

Attaching the buck converter schematics for reference.

CE Test observations:
Failing peaks observed in the low-frequency band, suspected to be related to the switching regulator fundamental and harmonics. (test results attached).

In addition, more Radiated emissions from 30MHz to 200MHz were also higher than the Class 5 limits.

Provide a suggestions to meet the CISPR25 class 5 Limit in the testing.

Hello,

It’s been a while. Your schematics look fine here. Here is the typical application for reference:

I feel that it would be more helpful to provide ways in improving your EMI performance if we perhaps took a look at images of your layout with these ICs. Hoping to hear back soon.

Best,

Krishan

In the meantime, here are some PCB Layout Guidelines for further reference:

Hello,

Please find the 3.3V buck layout in our board below,

Please find the 1.8V buck layout in our board below,

Hello,

For both layouts, I will make my comments with respect to the top power plane as shown in the PCB Layout Guidelines. Here is a zoomed in image of this:

Your layout could be more symmetrical here. I can see that you did this with Cin on both sides for the 1.8V and 3.3V layouts. However, trace widths could be further minimized here. Also are the SW and BOOT routed away enough from sensitive analog areas?

Hello,

We have routed the boot pin trace away from the sensitive signals.

Attached routing image for your reference.
Note: Here we have used the layer 3 for routing the boot pin trace. Our Buck chips placed in layer 8.

3.3V Buck:

1.8V Buck:

As long as there is some GND plane shielding between those layers, I would say that this change is ok.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.