We are using MPQ4323C to generate 12V from 24V power supply.
Issue description: During bench testing with a regulated DC power supply, the device failed when the input voltage was increased to 30 V DC. After the failure, a short circuit was measured between the pin SW and ground.
Could you please review the attached schematic and advise?
please let me know if you need any further information.
A short from SW to GND may be the integrated LS FET failing. The 30V is within the MPQ4323C’s absolute-max rating, so the input voltage itself is not the problem. The most likely root causes are:
SW-node ringing / overshoot: Any parasitic inductance in the SW loop (layout, inductor leads, BOOT path) will produce ringing that can exceed the SW absolute-max and destroy the LS FET.
Inductor saturation: If L100 saturates during a transient, the inductor current flows through the off-state LS FET at 30 V, exceeding its SOA. Please confirm L100’s saturation current rating is comfortably above the HS peak limit (~5.8 A) with margin for the max load.
Could you please share the L100 part number and, if possible, a scope capture of SW during the 24 V → 30 V ramp? That will help us narrow down whether this is a ringing issue or an inductor saturation issue.