Hi,
What is the voltage applied to the SS pin of this device?
In the reference schematic of the EVB datasheet, a capacitor with a 25V voltage rating is used. I am wondering if there is a specific reason for selecting a 25V-rated capacitor
Hi,
What is the voltage applied to the SS pin of this device?
In the reference schematic of the EVB datasheet, a capacitor with a 25V voltage rating is used. I am wondering if there is a specific reason for selecting a 25V-rated capacitor
Hi @sh_im ,
Apologies for the late reply; MPS had a company shutdown for the holidays. The SS (soft-start) pin has an absolute max rating of 5.5V, but you do not directly apply voltage to the SS pin. A capacitor (Css) is connected from SS to GND, and an internal 13uA current source charges Css at start-up. The voltage seen at SS pin is the voltage of Css.
SS, FB, and EA block:
More info on SS from datasheet:
Thanks,
Rubas
Hi, Rubas,
Thank you for your response.
I have an additional question: could you please explain why a capacitor with a 25V voltage rating is used?
Is it because the SS pin has an absolute maximum rating of 5.5V?
Hi @sh_im ,
A capacitor with 25V rating was most likely chosen by preference for its high voltage rating relative to the SS pin 5.5V absolute max rating. You can choose a lower voltage rating, but I recommend the capacitor having at least 10V rating (~twice the SS pin max rating).
Thanks,
Rubas
Thank you for your response. Although it’s a bit late, Happy New Year! Wishing you and your team continued success and good health in 2026.
This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.