Mpq4316gre-33-aec1-p

My customer got boards where I used MPQ4316GRE-33-AEC1-P, I put also 100K and 31K6 if use ADJ version. Customer measured 5V and sent me picture. I can’t recognize from datasheet is it 3.3V, 5V or ADJ version

MPSP40
MP4316
4B131B
E

Best regards,
Darko

Hello @ilic.darko,

Welcome to MPS forums. The MPQ4316-33-AEC1-P is designed for fixed 3.3 V output without having external resistors on the board. Please share the schematic of the board where 5 V was measured.


Here is they measured 5V on TP22 output

Hello @ilic.darko,

Thank you for sharing this schematic and top marking. The schematic shows the output as 3.3 V. For 5 V output, please change R54 to 19.6kohm.

I need 3.3V output, but they measure 5V which is wrong. NEED 3.3V OUTPUT as per schematic, but why has 5V?

Hello @ilic.darko,

Please remove the FB resistor divider and connect FB pin directly to the output as shown in the typical application circuit

Please let me know if this resolves the issue.

Thank you. According to mark on chip is it 3.3V version?

Hello @ilic.darko,

It should be 3.3 V version as long as the Vout is 3.3 V without the FB resistors.

Hello @ilic.darko,

This part is indeed a fixed 3.3 V output version of the MPQ4316.

Thank you @Saquib.FAE

1 Like