Hi MPS Team!
I wonder if there is any chance to get a SIMPLIS model for the MPQ4313-AEC1, converter.
The main purpose is to use SIMetrix/SIMPLIS Classic, to simulate the impact on the stability of the converter when a PI-Filter is placed at the input.
Despite DCDC Designer is super usefull, there is no option to modify the circuit simulated.
Thanks in advance for your support!!
Hi Pere,
The model is available within the MPSmart software,

Here is the link to download:
MPSmart | Design Tools | MPS | Monolithic Power Systems
Best,
Nouman
Hi Nourman,
Thanks for your answer, very usefull, this is great.
Eventhat, I can not find the MPQ4313, only the MPQ4323.
Can I use MPQ4323, being 100% representative of MPQ4313?
If not, is planned to get a model for the MPQ4313?
Thanks for your support!
Hi Pere,
My apologies on mis-reading the part name, unfortunately we do not have a simplis model to share at this time.
The two are not 100% same, pin out and configurability wise. 4313 is more configurable based on which specific the designer wants to have control over. You may compare by scanning through the datasheets.
Is there a specific reason you are going with MPQ4313-AEC1?
Best,
Nouman
Hi Nouman,
Yes to operating range for the iput voltage is the widest one.
But simulation wise, our intention is to integrate the SIMplis model with the a PI filter, to double check stability.
No worries, we can survive with the model you proposed, I just would like to know if it’s planed to provide the MPQ4313-AEC1 model, and by more or less when?
Thanks for your support!