MPQ4263GQVE-0002-AEC1 I2C configuration

Hello,

I have replicated the above schematic using MPQ4263GQVE-0002-AEC1 part number, and I am unable to see any output when I’m operating with same input voltage range provided in the datasheet. Could you kindly clarify if MPQ4263 0002 variant warrants a compulsory I2C configuration to see expected output. If so, what are the parameters that has to be configured through I2C (ie., VOUT, Frequency, EN etc)

Although the EN pin is held at 3.6 V in the above schematic, the datasheet link below on page 29 of MPQ4263 document states that the output is controlled by the operation command bit and must be set to enable the output on/off.

https://www.monolithicpower.com/en/documentview/productdocument/index/version/2/document_type/Datasheet/lang/en/sku/MPQ4263GQVE/document_id/10991/

Also, does the MPQ4263GQVE-0002-AEC1 come with a preset frequency or should that be enabled from the I2C configuration.

Thanks in advance for your help!

Hello @nuts1537

Thank you for posting your question in the MPS Technical Forum.
The MPQ4263-0002 defaults the OPERATION Register (01h) as ‘0’ (OFF).
Therefore, you will need to toggle this register value to ON via I2C.

Also, the switching frequency is preset to 280kHz, and the output voltage to 5V.

Regards,
Edgar

Hi,

Thank you for your response.

I am attempting to implement current limiting using the register configurations specified in the MPQ4263 datasheet. As mentioned in the datasheet, the current-limit function is expected to operate only in Forced PWM mode. However, during testing, the expected current-limiting behavior is not observed in either Auto PWM or Forced PWM modes.

Test Setup and Configuration:

  • VOUT set to 5 V with a DC electronic load connected

  • Current-limit threshold configured to 0.7 A

  • LDC disabled

  • CC enabled with CC blanking timer set to 3 ms

  • Operating modes tested: Auto PWM and Forced PWM

  • Sense resistor value: 5 mΩ

Observed Behavior:

  • Load current exceeds the programmed current limit, suggesting that CC mode may not be engaging

  • IMON pin remains at 0 V even when the load is drawing significant current

Could you please advise on the recommended next steps to debug or validate the current-limit functionality, or let us know if there are any additional configuration requirements or checks we should perform.

Thanks in advance for your help!

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.