We are considering the MPQ4242GVE-0015-AEC1-Z for a new design.
The datasheet indicates that “-0015” is an OTP-programmed configuration, but the specific settings are not described.
Could you please provide the details of the OTP configuration for the “-0015” version, including the USB PD profiles and any differences from the standard “-0000” version?
We would like to confirm whether this version meets our application requirements.
After reviewing the -0015 suffix in the MPQ4242 datasheet, I can only see the default -0000 suffix outlined.
To directly receive the full configuration file of the -0015 suffix from an FAE, please submit a ticket to the following link: Contact MPS - Design Assistance
OTP configuration details are worth checking carefully against the latest datasheet and programming procedure before committing settings. I’d also verify the required configuration values on a test unit first. For older electronics projects, sourcing parts such as Buy EOL CXA1364R SONY IC may similarly require careful verification of compatibility and specifications.