I’m currently working on a commercial battery-backed power supply project. Its main functionality is to provide a USB-C output with a custom 5V/5A (25W) Power Delivery profile designed for use with a Raspberry Pi 5.
For development purposes, I’m using the following setup:
– Evaluation board EVQ4242-VE-00B
– MPS USB-to-I²C dongle (EVKT-USBI2C-02)
– Virtual Bench Pro 4.0 software
The problem I’ve encountered is as follows (see attached image):
The official 27W USB-C power supply for the Raspberry Pi, when connected to the Pi 5’s USB-C port, continues broadcasting PD Source_Capabilities messages on the CC lines for at least 5 seconds after power-on. After this period, the Pi 5 firmware is able to negotiate PD and successfully request the 5V/5A profile.
In contrast, the MPQ4242, in its default configuration, only transmits PD messages for about 2.6 seconds before entering sleep mode. Such a shorter timing prevents proper PD negotiation of the Pi 5 and it falls back to the default 5V/3A profile.
My question: How can I configure the MPQ4242 to extend its PD broadcast duration from the default ~2.6 seconds to at least 5.2 seconds?
The datasheet only mentions: “The USB PD engine can disable the clock and enter sleep mode if no PD command is detected.”
I’ve searched for references to an “extra delay” or “timer” setting, but found nothing so far.
The MPQ4242 is otherwise an excellent fit for my application: it’s standalone, requires no additional MCU, and integrates both a PD source controller and a regulated buck-boost converter. This makes it one of the most attractive solutions on the market for designs without firmware development.
So far, I also haven’t found yet any other MPS devices that support both standalone PD source mode and custom 5V/5A profiles while maintaining PD broadcasts for >5 seconds.
Any guidance would be greatly appreciated. Thanks in advance!