Hi,
we would like to test thermal propertise of the eval board when external MOSFET is on.
According to the data sheet the RdsON settings must be close to the real RdsON @10V.
Since the MOSFET data sheet features typical and maximum values for the RdsON , given at 25° and 125°C , could you suggest what value should be set in the register CTL_SYS16 (0x2D), bits 4-6 EXT_HS_FET_RON?


Br
Josko
1 Like
Hello Josko,
We are currently looking into this matter. I will get back to you soon on this. Thank you for your patience.
Hello again Josko,
Apologies for the delayed response, bandwidth has been tight.
As the datasheet says, the EXT_HS_FET_RON should be as close to the in-application RDSon as possible. Reading the datasheet, you have a typical RDSon of 5-6.1 mOhms. Therefore, I would suggest that you have the EXT_HS_FET_RON = 0b001, corresponding to 5mOhms.
This is assuming you won’t be operating close to the max temp thresholds close to 125 degrees Celsius.
Best,
Krishan
This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.