Hello,
We developed a charging electronic for a tablet with the MPQ4242. Our intentional usecase would be, that the developed device is a USB data sink and a power source.
The charging is working fine up to 60W as expected.
We left the USB lines free since it is necessary for the charged tablet to also communicate via USB 2.0 to the device. When I connect the tablet via a USB 2.0 Type-A to Type-C cable, the USB connection works as intended.
Therefore, we assume that via the CC lines, the MPQ4242 is only recognized as a power brick. We also wrote to the “HOST_SET” register at 0x02 so that it should behave as a PDUSB hub, but still, only charging is possible when connected via USB-C.
Additionally we modified register 0x16 and enabled CDP. This also didn’t solved the issue. I also connected the USB lines for testing, but still no succsess.
Is it possible to use the MPQ4242 to communicate via USB 2.0 and charge with USB-PD in parallel? How can this be done?
Best regards,