MPQ4242 Behavior with OTW1, OTW2, and NTC Functions

Dear MPS Support Team,

We are currently using the MPQ4242BGVE-0017 model from MPS, and we are trying to use the OTW1, OTW2, and NTC functions.

Goal:

Register Configuration:

Our Settings
PDO
addr value
0x00 0x3f PDO_SET1: enable all PDOs
0x01 0x3a
0x02 0x60
0x03 0x96
0x04 0x5a
0x05 0x00
0x06 0x96
0x07 0x21
0x08 0x6e
0x09 0x3c
0x0a 0xc8
0x0b 0x00
0x0c 0xfa PDO_I4: PDO4 Current 5 A
0x0d 0x21
0x0e 0x6e
0x0f 0x3c
0x10 0x21
0x11 0xa0
0x12 0x3c
0x13 0x21
0x14 0xd2
0x15 0x3c
CTL
addr value
0x16 0x10
0x17 0x05
0x18 0xd9
0x19 0x4a PWR_CLT2: OTW1: 105 ˚C
0x1a 0x02
0x1b 0x1f
0x1c 0x48
0x1d 0x00
0x1e 0x01
0x1f 0xe8 GPIO1: IMON mode / GPIO2: NTC mode
0x20 0x36
0x21 0x84
0x22 0x23
0x23 0x36
0x24 0x84
0x25 0x1e
0x26 0x84
0x27 0xa0 OTW1_PDP: 80 W
0x28 0x3f OTW1_PDO_SELECT: enable all
0x29 0x3c OTW2_NTC_PDP: 30 W
0x2a 0x3f OTW2_NTC_PDO_SELECT enabel all
0x2b 0x0f
0x2c 0xe8
0x2d 0x04 OTW2: 115 ˚C
0x2e 0x5b NTC: Power Down mode
0x2f 0x32
Status
addr value
0x30 0x04
0x31 0x00
0x32 0x1e

The Results from our testing:

1. OTW1 Behavior

We set the maximum output power of PDO4 to 100 W (PDO4: 20 V / 5 A), and then tested by changing the OTW1 maximum power (OTW1_PDP, 0x27) to 80 W and 60 W.

  • When OTW1_PDP is set to 80 W, we confirmed that once OTW1 is triggered, the MPQ4242 controls the power to the specified maximum level (80 W). (PDO 3, max power 80 W was selected.)

  • However, when OTW1_PDP is set to 60 W, OTW1 triggering causes the system to repeatedly loop through the following sequence:
    (20 → 40 → 60 → charging stops → 20 → 40 → 60 → charging stops → …)
    Could you explain the reason for this behavior?


2. OTW2 Behavior

We found that even when OTW2 occurs, the output is not controlled according to the maximum power value configured for OTW2 (OTW2_NTC_PDP, 0x29).

  • Although the OTW2 Status bit is set, the power does not change to the configured OTW2 limit (30 W).

  • We tested two conditions:
    (1) OTW1 enabled and OTW2 enabled
    (2) OTW1 disabled, OTW2 enabled only
    In both cases, althought the OTW2 Status bit was set, the MPQ4242 did not change the power to the OTW2 maximum setting.

  • In our register configuration, only the following settings were changed for OTW2:
    OTW2_NTC_PDP (0x29) → 0x3C
    OTW2_NTC_PDO_SELECT (0x2A) → 0x3F
    Is there any incorrect configuration in these settings?


3. NTC Shutdown Mode

We would like to confirm the expected system behavior when NTC shutdown mode occurs.

  • When NTC shutdown is triggered, we observed that all MPQ4242 status register values stop updating. Is this the correct and intended behavior?

  • Should VBUS charging be completely disabled by the MPQ4242 when NTC shutdown occurs?

  • Is there any possibility that the MPQ4242 chip may be damaged when NTC shutdown mode is activated?


The Register bit field information for our settings is shown below, captured with no USB-PD connection:

We have a substantial number of MPQ4242 chips and want to ensure that we are using them correctly, and we would appreciate your support in resolving the issues we have observed.

Could you please review our register settings and usage scenarios to confirm whether there are any misconfigurations or incorrect operational assumptions?

Thank you.

Hi,

I’ve reached out to the local MPS Korea support team. They should be able to assist you with your queries soon.

Best,

Tyler