MPQ4241 for dual port charger

Hi,

We are developing a 36W shared output charger with dual ports being USB-A QC 3.0 and USB-C PD 3.0. Will the power sharing function be able to perform as intended if both ports are not USB-C. If not what are my alternatives to perform the same. I want each port to be able to draw 36W or share the 36W between the two ports as well. The Vin bus voltage is a constant 22V but can be changed to suite the design.

Regards,

Pratheek.

Hi,

Please fill out the MPS NOW Technical Support form. A member from the MPS NOW team will contact you within 24–36 hours about this request. Contact MPS - Contact

Best,

Fox

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.