Hi there!
I would like to change the output voltage, but without disabling it. The user manual there is method for it, but it mentioned to write ENPWR bit to 0 first (then write Vref, set Go_BIT=1 and then write ENPWR to 1).
Is it possible not to set the ENPWR bit to 0 before (or under) the change?
I would like keep always on the output voltage so the ENPWR bit should be 1.
Is there any problem for this method?
In the USP PD protocol the output voltage couldn’t drop beetween PDO changes, this is the main reason for the question.
Regards,
Bence