MPQ3446GUE-0002-AEC1 ic output voltage set configuation

Hi, we’re using the MPQ3446GUE-0002-AEC1 (12 V → 24 V boost, I2C). The public datasheet’s DVS_VOUT table doesn’t match this part: with power-on values (USER00 0x3008, USER01 0x1B21, USER02 0x50CD) it regulates at about 18.9 V, not 55 V. Writing the datasheet’s 24 V codes (0x7C or 0x80) stops switching entirely (BG flat, VOUT = VIN − diode). I2C is verified (no errors, byte order confirmed). Could you send the -0002 register map / OTP defaults and tell us which DVS_VOUT code gives 24 V?

Thanks!

Hi @gkarthik ,

Thank you for reaching out on the MPS Technical Forum.

I can confirm that the initial power-on values are supposed to regulate the MPQ3446 at 55V and the 24V codes you attempted to write should give you the correct output voltage of 24V.

To help troubleshoot your issue, are you able to share the schematic of this part? Furthermore, when programming the MP3446, are you using the MPS GUI or your own I2C interface?

Best,

Ryan

Hi Ryan,

No, I am not using the MPS GUI i have my custom board built with a microcontroller interfacing with the MPQ ic over i2c. Please refer to the schematic attached.

Thanks,

Karthik.

Hi Ryan,

The switch Q4 is placed wrong in the schematic, that is a known error and has been fixed in the board assembly. Please ignore that.

Thanks,

Karthik

Hi Ryan,

Can you share some insight about the issue faced ?

Thanks,

Karthik.