Hi MPS team, I would like to know if the LED channels of the MPQ3324 can be connected in parallel to drive a single LED string at a higher current.
My application requirements are,
Input Voltage - 5 V
Iset Current - 100mA
Desired LED current - 200mA
My main question is whether the MPQ3324 supports paralleling LED channels to drive a single LED string.
If this configuration is supported, are there any specific requirements regarding current sharing, channel configuration, or protection features?