Hi Team, I would like to use the MPQ2177GQHE-AEC1-Z in our design. Our Vin= 3.3V, Vout= 1V, Load current is 500 mA. Kindly review it and let us know
any feedback on the same.
Hello @abdul.rahuman,
Welcome to MPS Forums. Please connect the output pin to the load and not SW pin. The rest of the schematic looks fine but please verify the component values via equations in Application information on page 20 in the DS.
Hello @Saquib.FAE ,
Thanks for your comments. We updated the mistake & Kindly review it and let us know any feedback on the same.
Hello @abdul.rahuman,
Now the schematic looks correct to me.
Hello @Saquib.FAE,
One more query regarding this MPQ2177GQHE-AEC1-Z, can we use 47K in PG pin instead of 100K.
Hello @abdul.rahuman
I would recommend using 100k as a pull up on the PG pin as the resistance should be large enough to limit the current, so the internal MOSFET is not damaged.