Dear Sir/Madam,
I am not sure will it be damage MPM82504 when the circuitry configuration mismatched with factory code configurations.
Below is the case.
Ordered Part# with -0000 suffix (4 rails, 25A, different output voltages) solder on a PCB with the circuitry design in 2 rails application (0.85V @75A, 1V @25A, datasheet P.56 Fig. 11).
CTRL1~3 shorted with 10K pullup to VCC1~3 and CTRL4 with 10K pullup to VCC4 for native power-up application. There are two GND short jumpers at CTRL1~3 & CTRL4 to force DC-DC disabled by manual for onboard MTP programming.
In case power up the board without jumpers insert and without custom MTP programming, will it be damage this DC-DC Module while internal register configuration different from physical circuitry?
Best regards,
Ping