MPM54524 thermal model (.pdml format)

Hi Sir

Could MPS provide the thermal model (.pdml format) or any tool for thermal simulation? Or MPS can provide the power loss as setting below?

  1. Vin = 12V
  2. Vout = 3.3V
  3. Switching frequency = 750kHz
  4. Load current is 2.5A/3.3A for each loop

I just found this snapshot from the spec, but this setting is not what we want.
MPM54524

Hey Tim,

It looks as if the MPM54524 doesn’t have any curves characterized at Vin = 12V, Vout = 3.3V, and where Fsw = 750kHz.

However, generally the switching losses increase with a higher switching frequency, so it would be expected that the power loss would be where Vout = 3.3V @ Fsw = 750kHz would be somewhere in between the yellow and blue curves. You can use the data here as a worst-case approximation.

Of course, you could try running some simulations using the MPSmart tool as well. You can find the model online under the design tab on the following link:
MPM54524 | Fully Integrated, 16V, Quad 5A Output Power Module with I2C Interface | MPS

Hope this provided some insight.

This topic was automatically closed after 2 days. New replies are no longer allowed.