MPM54524 IC gets an UVLO error and 0 Volt output even after the proper input voltage

Hi,

We have used the two MPM54524 power module with i2c interface. I have configured the IC with the following configurations using the MSP430f677A.

In U1 (as per schematics attached below) IC, I have written the following
VOUT_RANGE_SELECT (25h) - 0x0F (sets the volt range to 1.2V to 3.6V with 15mV/step)
BUCKA_VOUT (15h) - 0X8E (sets the Output_a value as 3.33V)
BUCKB_VOUT (16h) - 0X8E (sets the Output_b value as 3.33V)
BUCKC_VOUT (17h) - 0X8E (sets the Output_c value as 3.33V)
BUCKD_VOUT (18h) - 0X8E (sets the Output_d value as 3.33V)
MONITOR_EN_REG (10h) - 0X0C (monitoring output_b voltage)
BUCKX_CTRL_REG (0Ch) - 0xFF (Enables all buck output regulator and sets it in a automatic mode)

Reads the following
STATUS_0 (00h) - 0x3c - (Every output is power not good, other than Buck_B)
STATUS_0 (01h) - 0x0b - (other than Buck_B, other outputs shows UVLO error)
BUCKX_VOLTAGE (06h) - (While powering on the IC, this register reads 0V. If I reads the register while the IC is in ON condition, I reads 2.7V only on Buck_B output. But, the measured output voltage is 4.45V in Buck_B output pin)
PART_ID (31h) - 0x24 -(as per datasheet)
OC_STATUS_CLEAR (2Ah) - 0x0F -(datasheet mentions it as a over current error

In U2 (as per schematics) IC, I have written the same but

Reads the following
STATUS_0 (00h) - 0x3c - (Every output is power not good)
STATUS_0 (01h) - 0x0f - (Every outputs is shows a UVLO error)
BUCKX_VOLTAGE (06h) - (Reads 0V)
PART_ID (31h) - 0x24 -(as per datasheet)

Now, I got 4.45V at Buck_B of U1 IC, Also its not responding based on the value set at BUCKB_VOUT, there is no change even after disabling the pin. Even other pins shows 0V and not responding to BUCKX_VOUT register. Kindly help me to sort it out.

Thanks and Regards,
Santhosh.

Due to the external voltage dividers, there found an errors. Now removed all external dividers and its working fine without errors.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.