MPM54322 Power ON Delay - not functioning query

Experimenting on a EVM54322. Would like to delay Buck 2 output until after Buck 1 is up.

I am having difficulty in getting any Buck 2 Power On Delay.
With the extreme values set below, we get no delay as shown in the scope cap.

We are using EVKT-USBI2C-02 and Virtual Bench Pro 4.0 v4.0.66.2007.

I have saved to Mode 0 region and verified the correct values are in the MTP region after power cycle from the GUI and individual reg read. The same ‘no delay’ waveform is seen at power-on and EN disable/enable. I have tried various other values of clock and Power On Delay with the same results.

Any suggestion where we are going wrong please?

Best wishes

Hi,

I think the blue curve is the Vout1 and the yellow curve is Vout2. There is a delay between these two outputs. You can zoom in the window to see the delay.

Best,

Fox

Hi Fox, Thanks for the reply. With the clock frequency set to 100Hz, the cycle time I’m expecting is 10ms. With a Power On Delay set to 1024, I’d be expecting a delay of around 10 seconds. Is that a correct interpretation of the Power On Delay function?

CH1 (Yellow) = Buck 1. CH2 (Blue) = Buck2. The scope cap above shows any delay is in the order of microseconds.