Hello,
Please can someone help me with programming MP54304 dev board - I lost two boards already as while programming the status shown ROM programmed but when power cycle still default Values .
I have bought 3rd dev board now and do not know how to proceed with this and make sure board is programmed.
Setup:
Board
EVM54304-MN-01A
Vin = 12V
EN switch OFF
Virtual Bench 4.0
Dev board has preprogrammed Vout without FB resistors , I want to program all BUCKS to use Vref 600mV and add FB resitors.
Please can you help and guide through Virtual Bench and to make sure I can program the ROM .
Thanks