Hi, can you suggest, R1 and R2 value if I need output 0.6V in the desgin? Thanks
Hi Izha,
Thank you for utilizing MPS Technical Forum,
I do not believe the 0.6V output can be supported with this device, it is quite low. Can you please provide me your input/output requirements so we can provide you with an alternate recommendation.
Note - the feedback network to set the output voltage uses the following equation for future reference.
Regards,
Nouman
Hi, thanks for reply
the datasheet writes, adjustable output from 0.6V
I suppose direct feedback from Vout without R2 should support 0.6V
Can you tell the minimum output it could support, if its not this case?
Hi Izha,
Apologies about late reply,
For an output of ~0.62V or 0.63V, you can try using the following feedback network.
R1 = 50k
R2 = 1M
Kind Regards,
Nouman