MPM3698-0000 Power Good Mode

I am using the MPM3698-0000, and I have an external pull-up resistor connected to the VRRDY pin. However, the VRRDY pin stays Low even when the output voltage is correct.

When I changed Rail2 → POWER GOOD MODE from the default Intel mode to POL mode, VRRDY started outputting High as expected once the output voltage was correct.

My question is:
Is this configuration change actually required?

Since this IC has only a single output, I originally assumed that all Rail2-related settings could remain at their default values, so I did not modify any other Rail2 parameters.

If changing the PG mode is necessary, are there any other Rail2 settings that also need to be adjusted from the defaults?

Thank you in advance for your support.

I’ll add a little more information.
The VRRDY1 and VRRDY2 pins are shorted together.

This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.