We have recently had issues with the MPM3683-7 powering down during operation.
This would power up correctly (Vin=3.5V, Vout=1.2V), but after running for few minutes to a few hours it would power off down to zero volts. Vin is still there, but Vout=0. Sometimes I can cycle the power and it would come back, but it would still do the same thing. Other times, it won’t come back.
I have replaced the part and then it seems to work as normal.
Can you check my schematic:
I have a few questions:
- should the SW pins be tied together or can they be left unconnected (I followed your layout recomendation of leaving them unconnecte?
- Is the external bias connection correct the way I drew it on the schematic?