Hi MPS team,
At he moment we are using the MPM3682-7 to convert 5v to 0.9V. This part is NRND and to mitigate the risk we are looking at the MPM3683-10.
I have already found that the footprint is different and the output current is higher. Are there any other specification differences between these parts that I should consider?
Best regards,
Michel Wouters
Hello Michel,
Other than the footprint and the higher output current at 10A, here are some other differences between the MPM3683-10 and MPM3682-7:
For the MPM3683-10, the max recommended input voltage here goes up to 16V whereas the MPM3682-7 goes up to 18V.
For the MPM3683-10, the thermal junction resistance is 5.1 degrees Celsius per Watt whereas the MPM3682-7 has 6.3 degrees Celsius per Watt.
Quiescent current is 650uA for the MPM3683-10, 860uA for the MPM3682-7.
Shutdown current is 10uA for the MPM3683-10, this figure is not specified for the MPM3682-7.
MPM3683-10 has selectable switching frequencies at 600kHz, 800kHz, and 1MHz where MPM3682-7 is programmable switching frequency from 200kHz - 1MHz.
See the efficiency graphs between these two modules. The MPM3683-10 is marginally higher in all cases.
There are many small differences as well, but these would be the more notable ones that can factor into your design.
Hope this provides some insight.
Best,
Krishan
system
Closed
June 25, 2026, 6:27pm
3
This topic was automatically closed 90 days after the last reply. New replies are no longer allowed.