Dear MPS’s technical support
I would like to know the change of output current versus temperature for the MPM3630GQV-Z model. It cannot be found in the current datasheet. For example, I want to know if the maximum output current at 85 degrees falls below 3A.
Best regards
Hello,
Are you referring to this below?

Best Regards,
Yu
Hello
No. I want to know maximum avaliable output current verses temperature.
For example, how much current can the MPM3630 output when the ambient or junction temperature is 85 degrees?
Best Regards,
Shinyoung Kim
Hi Shinyoung,
The recommended operating junction temperature is up to 125 deg C so at 85 deg C, it will still be able to handle 3A continuous current.
Best Regards,
Yu
Hi Yu,
Thank you for prompt reply!
Best Regards,
Shinyoung Kim